MAX6070AA_UT50+_A1: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX6x
MAX6070AA_UT50+_A1: FAQ
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
使用MAX6070A产生5V输出时,输出电压跟随输入电压变化,当5.3V输出时输出电压会变成5.2V。请问是什么原因?
MAX6070A电压基准具有非常高的输出电压精度,5V输出时精度达到0.04%,当输入电压超过5.06V时就应该能稳定在5V输出。如果不能够稳压,有可能是如下原因造成: 1. OUTF和OUTS没有短路到一起,导致内部环路断开,输出跟随输入变化。 2. MAX6070A可支持的最大输入电压为5.5V,极限电压为6V,如果电源上电时有高压过冲会导致器件损坏,造成无法稳压,因此要确保施加到器件上的电压不要超过5…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.