MAX38888ATD+_T1: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX3x
MAX38888ATD+_T1: FAQ
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
MAX38888可否用于电池管理
MAX38888是设计用于超级电容supercap管理的电源芯片,可以提供充电,逆变等功能。 由于其充电限制电压范围可设置为0.8V-4.5V,逆变电压可设置为2.5V-5V,故也可以用于电池类备份管理,实测参考Evkit: 1. 按照电池满电压/空dian'ya调整R1相关分压电阻值。 2. 调整R5值使逆变电压满足系统电源要求,可略低于外部电源值,以保证有外部电源时电池不逆变…
MAX38888电感值的选择和RISET的关系?
下面是RISET和电感选择的推荐值: L (µH) RISET (kΩ) 1 to 1.5 20 to 30 2.2 30 to 45 3.3 45 to 70 4.7 70 to 100 为确保可靠工作,建议客户按照推荐的值来选择电感。
MAX38888针对12V系统的应用方案
MAX38888是一款针对以超级电容作为备份电源的系统供电方案。当系统主电源供电并高于最低系统电源电压时,MAX38888将对超级电容进行充电,充电电流可达500mA。超级电容充电则保持就绪状态;主电池移除后,MAX38888内部DC-DC稳压器将电容电压转换为系统供电电压,可提供最高2.5A的超级电容放电电流。但MAX38888仅支持2.5V-5V供电系统。对于12V供电系统,可利用下述方案: …
多个MAX38888可以并联使用嗎?
MAX38888是不支持并联的。 如果并联的话,当两个不同步时会有问题,会发生过载而关断输出。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.