MAX1932ETC/GG8_T1: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX1932ETC/GG8_T1: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX1932是如何使用内部DAC设置输出电压的?
MAX1932的输出电压调节原理如下: FB处的电压是固定的1.25V,而从输出电压Vo到FB的电流等于从FB流到DACOUT与FB流到地的电流之和。而DACOUT处的电压可以通过DAC来控制,所以从FB流到DACOUT的电流是变化的,从而输出电压也是可以变化的。输出电压Vo的计算公式如下: (Vo-Vfb)/R5=Vfb/R8+(Vfb-VDACOUT)/R6,其中Vo为输出电压;Vfb为引脚FB的电压…
MAX1932最大输出电流是多少?
MAX1932用于产生APD偏压,高压输出(高达90V),电流最好限制在2.5mA以内。
如何扩展MAX1932的输出电压?
MAX1932的CS+、CS-引脚额定电压为+110V,增大输出电压( > 90V)对器件存在潜在的风险。我们也不建议在CS+、CS-引脚加分压电阻解决这一问题,因为CS+与CS-之间的检流电阻在0.5Mohm - 1Mohm之间,分压电阻的引入对环路稳定性有影响。我们不推荐采用以下电路提供高于90V的输出。 如需更高的输出电压,可以采用MAX1932 + 电荷泵的方案。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.