Article 如何将MAX17498BEVKIT的输入电压由5V改为3.3V

可以先将输出采样电阻R20由30.1kOhm改为16.9kOhm,此时输出电压在1.5A负载的情况下输出为3.3V,但是由于此时环路补偿并不稳定,会导致负载从0A到1A时输出电压不稳定。可以通过将电阻R15由1kOhm改为470Ohm解决环路问题。改完以后输出电压在全负载范围可以稳定在3.3V。输出电压纹波也没有出现振荡。

更改后的前后的效率及纹波测试曲线见附件。

总结:由于MAX17498B的变压器在设计时是按照5V输出来设计的,所以如果不更换变压器而直接更改输出电压会导致较低的效率。如果对效率要求较高,建议重新设计变压器。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.