MAX17498BATE+: FAQ

  • Created
Was this helpful?
  • MAX17498B内部MOS管开关时的上升与下降时间是多少?

    问题描述:MAX17498数据手册中,计算功率损耗时要用到内部MOS在开关时的上升时间tr与下降时间tf,为什么数据手册没有给出tr与tf的值? ----------------------------------------------------------------------------------------------------------------------------…
  • 为什么MAX17498B的输入电流为2mA,但是其内部LDO的输出限流值的典型值为100mA?

    内部LDO通常只给MAX17498B的内部电路供电,MAX17498B的内部电路消耗的电流比较小,此时MAX17498B的输入电流大概是2mA左右。而内部LDO还可以给一些外部电路供电,但是它能提供的最大电流只有几十毫安,如果超过50mA,则LDO会出现过流,输出电压不稳定。通常情况下,不建议LDO的输出接其它电路。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.