MAX17243: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX17243: FAQ
Created
over 8 years ago
Updated
3 months ago
Was this helpful?
Yes
No
More
Cancel
MAX17243可以产生20V输出吗?
MAX17243输出受限于器件的ESD内部结构,最大输出电压可设置为10V。
在使用MAX1724时,当管脚/SHDN接低电平时,MAX1724应该处于关断状态,没有电压输出。而我在实际使用的时候发现,当/SHDN接低电平时,MAX1724有电压输出,请问,如何才能完全关闭MAX1724?
MAX1724 shutdown 是指器件此时不工作,由于该器件不是真关断,因此,此时输入的电压会通过内部的 MOSFET 以及电感连接到输出,如果您需要真关断的升压器件 . 如果需要5V输出请参考MAX8627.
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.