MAX17225ENT+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX17225ENT+: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX17225的最大输出电流是多少?
MAX17225的最大输出电流是800mA,但是MAX17225并非在所有条件下输出电流都可以达到800mA。最大输出电流还与输入输出电压有关,例如在输入电压范围为1.4V到1.6V,输出为3V的情况下,最大输出电流是247mA。由于MAX17225的datasheet中很难给出在任意输入输出电压情况下的最大输出电流,可以使用EE-Sim仿真来得到任意输入输出电压情况下的最大输出电流,下面是EE-Sim的链接…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.