MAX16834: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX16834: FAQ
Created
over 8 years ago
Updated
2 months ago
Was this helpful?
Yes
No
More
Cancel
MAX16834外围元器件如何配置?
依照如下电路设计要求: 硬件平台:MAX16834EVKIT+ LED电压:111V (最大130V) 输出电流:1A 输入电源: 最大20V电压输出的电源(最大输出电流9A以上) 根据Datasheet进行计算,外围元器件参数选取如下: 开关管N2:Vds电压应大于160V (130V*1.3), 漏极电流应大于8.7A 电感L1:电感值4.2uH~42uH,饱和电流及RMS电流应大于8…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.