MAX16826最大电流限制是多少?
文档
Forums
Members
Tags
Cancel
Was this helpful?
Was this helpful?
Yes
No
In this Article
Created
over 8 years ago
Updated
9 months ago
文档
MAX1x
MAX16826ATJ/V+: FAQ
MAX16826最大电流限制是多少?
MAX16826支持的最大是4A, 也就是每通道1A。 如果需要2A,也就是每个通道500mA,器件可以满足要求。
以第一通道为例,R31=VCS/500mA
Vcs是97mV到316mV中的一个值,可以通过I2C来配置。
芯片的单通道的最大电流不超过1A, 电阻 值不小于VCS/1A.
电阻的功率是电流的平方乘以电阻值进行计算,这个可以根据贵司的设计规则和发热测试选择相应功率等级的电阻。
如果您的电感峰值电流是6.5A, 根据R12=200mV/(1.2*6.5A) 进行选型。
MAX16826
000096606
Power 中文专区
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.