MAX16826ATJ/V+: FAQ

  • Created
Was this helpful?
  • MAX16826典型电路中VIN和管脚IN之间的电阻有什么作用?是否可以移除?

    这个电阻用于限流保护。 MAX16826的IN引脚内部连接了一个26V稳压管,外部电源通过这个限流电阻接IN引脚,在发生汽车抛负载时,提供电压箝位和限流保护。电阻计算公式如下: 如果IN的供电电源小于5.5V,则可旁路内部线性稳压器,将IN直接连到VCC管脚即可,此时不用连接这个电阻。
  • MAX16826最大电流限制是多少?

    MAX16826支持的最大是4A, 也就是每通道1A。 如果需要2A,也就是每个通道500mA,器件可以满足要求。 以第一通道为例,R31=VCS/500mA Vcs是97mV到316mV中的一个值,可以通过I2C来配置。 芯片的单通道的最大电流不超过1A, 电阻 值不小于VCS/1A. 电阻的功率是电流的平方乘以电阻值进行计算,这个可以根据贵司的设计规则和发热测试选择相应功率等级的电阻。 如果您的电感峰值电流是6…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.