MAX16826ATJ+: FAQ

  • Created
Was this helpful?
  • MAX16826典型电路中,R20 - R27的作用是什么?

    MAX16826数据手册的典型电路中,MOSFET的漏极电压决定了故障状态。以下典型电路中的R20-R27分压电阻用于决定故障检测的电压。
  • MAX16826只能用于大电流LED驱动吗?

    MAX16826可以驱动4串LED,每串LED的电流由连接在MOSFET源极的检流电阻以及检流调整电压确定。电流调整电压默认值为318mV,通过I2C接口编程,调整步长1.72mV,范围:97mV-318mV。因此,并不局限于大电流应用。只是,如果LED电流很小的话,可以选择更简单的方案。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.