MAX16053AUT+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
MAX16053AUT+: FAQ
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX16053是否可以通过外部MOSFET用于使能电源通路?
MAX16053为高压电源排序器,带有高电平有效推挽式输出。输出用于驱动开关电源的使能引脚。但由于其输出电压取决于VCC,可高达+28V,所以往往被用于其他功能。输出也可用于驱动低边n沟道MOSFET的栅极,或者输出反相后用于驱动高边p沟道MOSFET的栅极。 如果输出直接连接到高边n沟道MOSFET的栅极,从漏极到源极的电压被限制到VCC - VT,其中VT为MOSFET的门限电压。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.