ADG
文档
Forums
Members
Tags
Cancel
文档
ADG
Created
1 month ago
Was this helpful?
Yes
No
More
Cancel
ADG33xx_PCB走线长度
对于ADG33xx系列产品,许多客户遇到有关驱动能力的问题。 我们是否有驱动电流和负载电容的详细测试值?PCB走线应当是多长?
ADG4612输入范围
我有一个关于模拟开关数据手册的问题。 最大导通电阻平坦度指的是什么?它与导通电阻有何区别? 期待您尽早回复。
ADG5436_不平衡电源
有一个关于ADG5436的问题。客户想利用单刀双掷(SPDT)开关产生-40V到0V的逻辑信号,因此他需要一个不平衡的电源。例如:Vss=-40V,Vcc=7V。然而,我认为这会超出ADG5436的电源范围。我不确定ADG5436或任何其它器件是否能支持该应用。 我让客户进行一些测试。
ADG918_P1dB点测试条件
我对输入电源感到困惑。我看到两个输入电源:0V偏置和0.5V偏置。同时我发现,1000MHz时的P-1dB为17dB。我的问题是:该P-1dB是在哪种偏置下测得的,0V偏置还是0.5V偏置?
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.