over 8 years ago
ADF
ADG
ADL
ADM
ADP
General
MAX1x
MAX2x
MAX3x
MAX5x
MAX6x
MAX7x
MAX8x
Was this helpful?
Yes
No
More
Cancel
Recently Updated Articles
ADM3053 隔离式CAN收发器带隔离电源
ADM3053 Isolated CAN Transceiver with Isolated Power Supply by zhc787 ADM3053 Isolated CAN Transceiver with Isolated Power Supply The ADM3053 is an isolated controller area network (CAN) physical layer transceiver with an integrated isolated DC/DC…
ADL5380 EVB中使用的巴伦
我有两个关于ADL5380的问题需要你确认。 1. 我想购买ADL5380的高频段EVB,评估板上焊接了何种巴伦?3600BL14M050、5400BL15K050还是仅提供尺寸?2. 如果ADL5380用于单端RFin和LOin(无巴伦),使用RFIP和LOIP,RFIN和LOIN交流耦合接地,单端工作的性能降级预期是多少?
MAX8815A 的5V输出电压精度是多少?
MAX8815A 的5V输出电压取决于输入电压与负载,可以通过MAX8815A的datasheet第4页的OUTPUT VOLTAGE vs. LOAD曲线来确定在不同输入电压与负载下的输出电压。
What does the MAX17227A do when the input voltage is greater than the set output voltage, but less than 1V greater than Vout ?
Q: What does the MAX17227A do when the input voltage (Vin) is greater than the set output voltage (Vout), but less than 1V greater than Vout (so that the short circuit protection does not activate)? Does Vin pass through to Vout, and if it does, what…
MAX6734的 VCC1 和 VCC2 可接相同電位嗎?
MAX6734 的Vcc1 和Vcc2應該分別接不同的電壓。不建議VCC1 和VCC2接相同電位,一般建議VCC2接比VCC1低的電壓。 IC 的供電會在VCC1 和VCC2之間自由切換成電壓較高的一側,如果VCC1,2接相同的電壓,則會導致 MAX6734的供電頻繁切換。 建議根據VCC2的電位選擇對應的尾綴的產品。
Most Helpful Articles
为什么MAX17498B的输入电流为2mA,但是其内部LDO的输出限流值的典型值为100mA?
内部LDO通常只给MAX17498B的内部电路供电,MAX17498B的内部电路消耗的电流比较小,此时MAX17498B的输入电流大概是2mA左右。而内部LDO还可以给一些外部电路供电,但是它能提供的最大电流只有几十毫安,如果超过50mA,则LDO会出现过流,输出电压不稳定。通常情况下,不建议LDO的输出接其它电路。
如何将MAXREFDES48#的输出更改为24V/2A?
可以将参考设计MAXREFDES48#做以下更改从而得到24V/2A的输出 1. 变压器 T1: 使用汉仁的HR102302 2. 电感L1: 使用Coilcraft的 SER1390-473ML 3. C12更改为 22nF, 比如 GRM31BR72D223KW01# 4. C1使用3个10uF 5. C17,C19,C20,C23使用10uF, 比如 GRM32EB31H106KA12# 6. N2,N3使用 SiSS40DN 7. R32: 550 kohm 8. R31: 3.5 kohm…
MAX17225的最大输出电流是多少?
MAX17225的最大输出电流是800mA,但是MAX17225并非在所有条件下输出电流都可以达到800mA。最大输出电流还与输入输出电压有关,例如在输入电压范围为1.4V到1.6V,输出为3V的情况下,最大输出电流是247mA。由于MAX17225的datasheet中很难给出在任意输入输出电压情况下的最大输出电流,可以使用EE-Sim仿真来得到任意输入输出电压情况下的最大输出电流,下面是EE-Sim的链接, http://maxim.transim.com/Loader/New.aspx
可否推荐配合 MAX86140/86141的LED和photodiode?
可以根据具体应用要求来选择合适的 led,photodiode,,以下为 推荐型号: •LED >OSRAM PointLED: LT P4SG •Photodiode >Vishay TEMD5010
MAX38902A的输出电压过冲是否可以控制在15mV以内?
可以,将典型应用电路中的输出旁路电容更换成1uF即可限制输出摆率,抑制输出过冲。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.