Post Go back to editing

ad9547配置问题,AD9547 configuration issue

Category: Software
Product Number: ad9547

我想利用AD9547产生两个输出,但是我看了数据手册不是明白,我想问我该如何配置ad9547寄存器?手册上还提到了一个eeprom,这个器件在芯片中是什么作用?

I want to use AD9547 to generate two outputs, but I didn't understand after reading the data manual. I want to ask how to configure the AD9547 register? The manual also mentions an eeprom. What is the function of this device in the chip?

  • ADI 提供 AD9547-EVAL GUI,可以离线完成寄存器的设置并通过 View -> Register Map Values Windows 查看相应值,以便对芯片进行编程。

    Useful link:UG-639

    AD9547 内置的 EEPROM 用于保存芯片配置参数,并能在设备断电重启后通过配置M3~M7引脚加载之前保存的数据,避免每次上电时重新编程,更多说明见规格书 EEPROM 部分的内容。