Post Go back to editing

DS1339U-33

Summary of the phenomenon of clock jumping from 11:59 to 4:00:
1. As long as there is no operation to set the time, the device runs normally, or it shuts down and starts up again, and the clock has not had any problems.

2. The clock was reset to around 10 o'clock, and when it ran to 11:59, the clock became 4:00 o'clock.

Parents
  • Are you using a homemade circuit board or an ADI evaluation board? Please provide the circuit board schematic diagram and operating steps, as well as any materials that are helpful for analysis, such as test conditions, test waveforms, etc.

Reply
  • Are you using a homemade circuit board or an ADI evaluation board? Please provide the circuit board schematic diagram and operating steps, as well as any materials that are helpful for analysis, such as test conditions, test waveforms, etc.

Children
No Data