Post Go back to editing

difference between LTC6946-3 and LTC6948-3

hello:

 our company using LTC6946-3 generate 800MHz from 16M source,  LTC6946-3  Will be discontinued soon, these two devices Pins are incompatible i want using LTC6948-3 to replace,  i want to know  Whether i  need to make very big changes code  about  the SPI driver code and Associated registers between these two devices, thanks a lot.  

Parents
  • LTC6946-3可以用LTC6948-3作替换,后者为分数频率合成器,但具备整数频率合成器(LTC6946-3)的功能,且能在较高频率参考信号下获得高精度的输出信号频率。SPI Driver Code改动不会太大,二者数据传输及读写时序基本相同,只需根据项目需求更改对应功能寄存器的值,比如:LTC6948-3在整数模式下的输出频率公式是否有所变化,与哪些量有关等,具体信息可参考LTC6948-3。相比Driver Code,硬件电路因管脚不兼容而需要作较大改动,可参考LTC6948-3规格书中的参考电路进行设计。

Reply
  • LTC6946-3可以用LTC6948-3作替换,后者为分数频率合成器,但具备整数频率合成器(LTC6946-3)的功能,且能在较高频率参考信号下获得高精度的输出信号频率。SPI Driver Code改动不会太大,二者数据传输及读写时序基本相同,只需根据项目需求更改对应功能寄存器的值,比如:LTC6948-3在整数模式下的输出频率公式是否有所变化,与哪些量有关等,具体信息可参考LTC6948-3。相比Driver Code,硬件电路因管脚不兼容而需要作较大改动,可参考LTC6948-3规格书中的参考电路进行设计。

Children
No Data