有一个ADF4159 MUXOUT输出的问题想问一下大家。
我用的是50M的参考时钟,分频器型号为ADF4159CCPZ-RL7,VCO型号为HMC1167,寄存器从R7到R0分别设置的是
0x7
0x6
0x5
0x4
0x384C3
0x7108002
0x1
0x181CC000
想在MUXOUT引脚R-DIVIDER模式输出25Mhz的频率,但是不论怎么修改R0寄存器,R-DIVIDER模式出来的都是1.56Mhz,咨询一下各位如何解决
求教,感谢
有一个ADF4159 MUXOUT输出的问题想问一下大家。
我用的是50M的参考时钟,分频器型号为ADF4159CCPZ-RL7,VCO型号为HMC1167,寄存器从R7到R0分别设置的是
0x7
0x6
0x5
0x4
0x384C3
0x7108002
0x1
0x181CC000
想在MUXOUT引脚R-DIVIDER模式输出25Mhz的频率,但是不论怎么修改R0寄存器,R-DIVIDER模式出来的都是1.56Mhz,咨询一下各位如何解决
求教,感谢
你好,我也在调ADF4159,你说的那个写入顺序指的是最后写R0吗?我现在R-DIVIDER以及R-DIVIDER/2都能测到信号,但是N-DIVIDER确测不到信号,N-DIVIDER/2能测到信号,这个你也遇到过吗?谢谢!
Hi,
Yes, there is an initialization sequence for the register write. You can check page 25 of the datasheet.
Best Regards,
Emrecan
Many thanks!
1、我也看到了R6寄存器STEP_SEL = 0 和STEP_SEL = 1,以及R5寄存器DEV_SEL = 0和DEV_SEL = 1。需要设置两次,但不清楚为什么?
2、MUXOUT配置为N-DIVIDER/2能测到500Khz的信号,R-DIVIDER测到1Mhz,但是N-DIVIDER为什么测不到呢?
参考时钟50Mhz,寄存器配置如下:
0x7
0x6
0x800006
0x5
0x800005
0x84
0xc4
0x1430003
0x42c800a
0x1
0x72ee0000
谢谢!
Duplicate question, already replied here:
ez.analog.com/.../480782
Duplicate question, already replied here:
ez.analog.com/.../480782