有一个ADF4159 MUXOUT输出的问题想问一下大家。
我用的是50M的参考时钟,分频器型号为ADF4159CCPZ-RL7,VCO型号为HMC1167,寄存器从R7到R0分别设置的是
0x7
0x6
0x5
0x4
0x384C3
0x7108002
0x1
0x181CC000
想在MUXOUT引脚R-DIVIDER模式输出25Mhz的频率,但是不论怎么修改R0寄存器,R-DIVIDER模式出来的都是1.56Mhz,咨询一下各位如何解决
求教,感谢
有一个ADF4159 MUXOUT输出的问题想问一下大家。
我用的是50M的参考时钟,分频器型号为ADF4159CCPZ-RL7,VCO型号为HMC1167,寄存器从R7到R0分别设置的是
0x7
0x6
0x5
0x4
0x384C3
0x7108002
0x1
0x181CC000
想在MUXOUT引脚R-DIVIDER模式输出25Mhz的频率,但是不论怎么修改R0寄存器,R-DIVIDER模式出来的都是1.56Mhz,咨询一下各位如何解决
求教,感谢
你好,我也在调ADF4159,你说的那个写入顺序指的是最后写R0吗?我现在R-DIVIDER以及R-DIVIDER/2都能测到信号,但是N-DIVIDER确测不到信号,N-DIVIDER/2能测到信号,这个你也遇到过吗?谢谢!
Hi,
Yes, there is an initialization sequence for the register write. You can check page 25 of the datasheet.
Best Regards,
Emrecan
Hi,
Yes, there is an initialization sequence for the register write. You can check page 25 of the datasheet.
Best Regards,
Emrecan
Many thanks!
1、我也看到了R6寄存器STEP_SEL = 0 和STEP_SEL = 1,以及R5寄存器DEV_SEL = 0和DEV_SEL = 1。需要设置两次,但不清楚为什么?
2、MUXOUT配置为N-DIVIDER/2能测到500Khz的信号,R-DIVIDER测到1Mhz,但是N-DIVIDER为什么测不到呢?
参考时钟50Mhz,寄存器配置如下:
0x7
0x6
0x800006
0x5
0x800005
0x84
0xc4
0x1430003
0x42c800a
0x1
0x72ee0000
谢谢!
Duplicate question, already replied here:
ez.analog.com/.../480782