I use the adf4355 board, download the corresponding software and driver according to the instructions, and change the frequency I want to output on the control panel. But no matter how I adjust, the output frequency is a value can not be changed
I use the adf4355 board, download the corresponding software and driver according to the instructions, and change the frequency I want to output on the control panel. But no matter how I adjust, the output frequency is a value can not be changed
Hi,
Because it's the first time I've ever used it, I haven't changed it.
The ones you circled are all there.
Zsq1
Thank you for the reply.
Which button do you use? 1 or 2? You should use Write Init button to initialize the part.
Regards,
Kudret
Hi,
I'm a little confused. Do I have to press button one every time? When I could not change the output frequency before, I pressed it, and the signal would not show on the spectrum instrument. I had to turn off the board and open it again, and then press button 2 to show the signal on the spectrum instrument.
zsq
Hi,
I just tried it again. When my board switch is not on, I press button 1 and turn on the board switch. The output is the same value as before. When I turn the board on, I press button 1, no matter how much I change the value in VCOout, I can't get a signal out, I had to turn the board off and back on to get the signal out.
zsq