Our lab bought 2 ADF5610 evaluation boards recently. We know how to use it to generate a frequence automatically(just click "write all registers"), but I don't know how to generate a specified frequency manually. I operate as follows:
1. disable "Autocal Disable"(Register 0x0A Bit[11]);
fig.1:
2. write a frequency in the "RF Output Controls" tap;
fig.2:
3. choose a subband in the "VCO Subsystem" tab;
fig.3:
4. click "write all registers"
As a result, in the Spectrum Analyzer, it shows two wrong Spectral lines(one around 7GHz, the other around 14GHz). No matter what frequency I write, the Spectrum Analyzer shows the two fixed wrong Spectral lines. So what is the right operation steps to let the ADF5610 generates a specified frequency manually. By the way, what is the relationship between "Autocal Disable"(Register 0x0A Bit[11], fig.1) and Cal(VCO Register 0x00 Bit[0], fig.2)? Looking forward to for your assistance.