问几个关于admv4530的问题

关于admv4530有几个问题想咨询下专家:

1,admv4530的参考输入是否可以使用200M的晶振

2,我的理解是admv4530是一个单芯片上变频器解决方案,看功能框图,RFOUT在输出时进行了两次放大,增益50db,RF增益和中频增益可调范围70dbm。这是不是意味着如果用admv4530设计上变频器,在输出后可以不用再进行滤波放大,信号直接给omt和馈源上星。

3,admv4530的IF输入范围是2G-3G,那如果调制解调器的中频信号范围是1850M-2300M,如何调整admv4530的IF输入.是不是通过设置调制解调器的BUC本振频率来调整还是用其他什么方法。

Parents
  • +1
    •  Analog Employees 
    on May 12, 2020 7:34 AM 11 months ago

    您好,感谢对ADI产品的关注。

    PLL的参考输入200MHz是典型值,其上限可以达500MHz.输入信号摆幅见手册的spec.

    输出功率的1dB压缩点可以参考手册的图21.如果达到了您的使用功率,外部不需要再增加功率。

    参考手册的图36,看起来IF 在1.85G转换性能稍微受到一些影响,但是也是可以使用的。

Reply
  • +1
    •  Analog Employees 
    on May 12, 2020 7:34 AM 11 months ago

    您好,感谢对ADI产品的关注。

    PLL的参考输入200MHz是典型值,其上限可以达500MHz.输入信号摆幅见手册的spec.

    输出功率的1dB压缩点可以参考手册的图21.如果达到了您的使用功率,外部不需要再增加功率。

    参考手册的图36,看起来IF 在1.85G转换性能稍微受到一些影响,但是也是可以使用的。

Children
No Data