多个ADF4351输出同一频率时如何调整相差

我期望用两片ADF4351实现两路相差可调的点频信号。如,设置信号频率为151MHz,相差45°。

目前,我已利用STM32f103RTC6做上位机控制两片ADF4351电路板,实现了两路同步的151MHz的单频信号。但是每次加电后输出的相位差都是随机的,请问如何控制相差?

ADF4351的“调整相位”、“相位再同步”这两个功能我都分别尝试过多次,无法达到控制相差的目的(不知道是不是我寄存器的值设的有问题)。

请问这个问题怎么解决?芯片手册我学习了很久了。手册上“相位再同步”部分的例子我也尝试过,结果是每次加电的输出相位差还是随机变化的。所以如果4351能实现这个功能,请告诉我R5-R0的6个寄存器的值设多少。

Parents Reply Children
No Data