Post Go back to editing

ADALM2000(M2K)模拟输出问题咨询

Category: Hardware
Product Number: ADALM2000
你好,我是通过libm2k中的api来控制ADALM2000。
问题:
      我所编写的代码首先将模拟通道1(M2K有两个模拟通道,模拟通道0和模拟通道1)配置为75MHz的采样频率,然后让模拟通道1输出100Hz的锯齿波一个周期,再将模拟通道1的采样频率配置为7.5KHz,令其输出范围为-1.96V~+2.16V的锯齿波,此时用示波器测该锯齿波的实际幅值为-2.64V~+2.88V的锯齿波,锯齿波的幅值显著大于我向M2K写入的锯齿波的幅值。
     如果不把模拟通道1采样频率配置为75MHz,而是直接将其配置为7.5KHz令其输出范围为-1.96V~+2.16V的锯齿波,此时利用示波器测其波形是正常的。
请问有什么方法能够让我在改变采样频率的情况下也能输出理想幅值的锯齿波吗?
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.