Post Go back to editing

Can the ADSP21569 accept a 24.576 MHz crystal oscillator?

I want to use 21569 sports as the master mode to transmit LRCK and BCLK to the external AD/DA. To ensure the audio sampling rate of 48 kHz or 96 kHz, I want to change the clock crystal oscillator of the DSP from 25 MHz to 24.576 MHz. Excuse me program CCES program inside also want to do corresponding modification? 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.