Post Go back to editing

AD9363杂散问题

您好!

我们在使用Zynq7030+AD9363的板卡做基带,发现在较高分辨率的情况下,AD送出的信号频谱质量很差,出现周期性的杂散,发送单音时有周期性的1M杂散,想请教下各位如何进行排查。

目前已知的情况是:采用了MUN12AD03-SH作为DC/DC,开关频率1M,但是也有使用ADP1755进行稳压。基带频率设置为9.6M,速率档分为150k,300k,600k,1.2M,杂散周期分别为16.2k,32.5k,65k,130k,单音测试为1M的周期杂散。

目前完成的测试包括:

1、通过使用外部时钟,杂散问题仍然存在;

2、通过回读寄存器,RFPLL和BBPLL是锁定的;

3、使用BIST测试,设置ad寄存器3f4为33时,情况如下,在更高分辨率下仍然出现有谐波;

4、确认接口时序,修改0x007的时钟延迟和发送数据延迟,无改善;

5、确认发送校准相位、增益和偏移矫正,无改善;

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.