In project 1, two boards, two hmc7043 chips per board, with a total of 16 channels, are verified. Each board corresponds to four 9680 chips, which are used for synchronization of multiple ad chips. The judgment condition is that the change of power on and power off phases of multiple chips does not exceed a certain range. If it exceeds, the judgment fails. Normal temperature and high temperature synchronization, low temperature test, two channels of a piece of AD and other ad chip synchronization error, error channel fixed. Through the test waveform, it is found that the output sysref (sclkoutx) of the error channel has a fixed difference of four sampling clocks compared with other channels, the clock input frequency changes, the number of sampling clocks of the difference remains unchanged, the phenomenon of the two boards is the same, the low temperature error occurs, but the error channels of the two boards are different. In addition, after replacing the 7043, the number of error channels becomes another channel corresponding to the chip. Error probability, one error every 8 pieces
Project 2: a total of 3, using a hmc7043 chip, two ad, also used for multi-channel synchronization, the phenomenon is similar, low temperature synchronization error, there was a difference of 16 / 32 / 64 sampling clock.
Project 3: one board card, one hmc7043 chip, four ad chips. The phenomenon is similar. There are four sampling points for a channel error.
Project Block Diagram:
Figure 2: Waveform in case of error (between any two SYSREFs)
Figure 3: Waveform in case of error (between any two SYSREFs)
Figure 4:Normal waveform (between any two SYSREFs)
Item 4 is similar to the above phenomenon. Low temperatures of -55 and -40 degrees are very prone to errors, almost every time, normal temperature is missed only once.The 7043 configuration as follows.
0x0 : 0x1
0x0 : 0x0
0xc8 : 0x0
0xd2 : 0x0
0xdc : 0x0
0xe6 : 0x0
0xf0 : 0x0
0xfa : 0x0
0x104 : 0x0
0x10e : 0x0
0x118 : 0x0
0x122 : 0x0
0x12c : 0x0
0x136 : 0x0
0x140 : 0x0
0x14a : 0x0
0x9f : 0x4d
0xa0 : 0xdf
0x46 : 0x0
0x50 : 0x0
0x5a : 0x7
0x64 : 0x1
0xc9 : 0x0
0xca : 0x0
0xd0 : 0x0
0xcb : 0x0
0xcc : 0x0
0xcf : 0x0
0xc8 : 0x0
0xd3 : 0x0
0xd4 : 0x0
0xda : 0x0
0xd5 : 0x0
0xd6 : 0x0
0xd9 : 0x0
0xd2 : 0x0
0xdd : 0x4
0xde : 0x0
0xe4 : 0x8
0xdf : 0x0
0xe0 : 0x0
0xe3 : 0x0
0xdc : 0xc1
0xe7 : 0x0
0xe8 : 0x0
0xee : 0x0
0xe9 : 0x0
0xea : 0x0
0xed : 0x0
0xe6 : 0x0
0xf1 : 0x4
0xf2 : 0x0
0xf8 : 0x8
0xf3 : 0x0
0xf4 : 0x0
0xf7 : 0x0
0xf0 : 0xc1
0xfb : 0x4
0xfc : 0x0
0x102 : 0x10
0xfd : 0x0
0xfe : 0x0
0x101 : 0x2
0xfa : 0xc1
0x105 : 0x4
0x106 : 0x0
0x10c : 0x8
0x107 : 0x0
0x108 : 0x0
0x10b : 0x0
0x104 : 0xc1
0x10f : 0x20
0x110 : 0x3
0x116 : 0xb0
0x111 : 0x0
0x112 : 0x0
0x115 : 0x0
0x10e : 0xcd
0x119 : 0x1
0x11a : 0x0
0x120 : 0x8
0x11b : 0x0
0x11c : 0x0
0x11f : 0x0
0x118 : 0x41
0x123 : 0x20
0x124 : 0x3
0x12a : 0xb0
0x125 : 0x0
0x126 : 0x0
0x129 : 0x0
0x122 : 0x4d
0x12d : 0x1
0x12e : 0x0
0x134 : 0x8
0x12f : 0x0
0x130 : 0x0
0x133 : 0x0
0x12c : 0x41
0x137 : 0x20
0x138 : 0x3
0x13e : 0xb0
0x139 : 0x0
0x13a : 0x0
0x13d : 0x0
0x136 : 0x4d
0x141 : 0x1
0x142 : 0x0
0x148 : 0x8
0x143 : 0x0
0x144 : 0x0
0x147 : 0x0
0x140 : 0x41
0x14b : 0x20
0x14c : 0x3
0x152 : 0xb0
0x14d : 0x0
0x14e : 0x0
0x151 : 0x0
0x14a : 0x4d
0xa : 0x3
0x5b : 0x4
0x5c : 0x20
0x5d : 0x3
0x1 : 0x2
0x1 : 0x0