AD9957正交上变频输出频谱有很高随机闪烁杂散

方案是FPGA+AD9957做上变频。AD9957配置为正交上变频模式,参考输入20M,系统时钟为内部PLL输出640M,DDS配置为140M,PDCLK频率为1/2模式,即IQ数据采用PDCLK上下边沿传输,PDCLK极性反转开启,内插滤波器因子为5,即PDCLK频率为640/(2*5)=64M,IQ数据采样率分别为32M。FPGA采用K7,内部用PDCLK引入DDS内核产生一个sin和cos信号,频率1M,再用DDR原语输出。现在的现象是在温度为几度时,AD9957输出信号两边几十M带宽内有随机闪烁杂散出现,而且温度越低,杂散越多越强,到零下-40度,频谱已经是一个噪声带了。高温的时候特别好,频谱很干净,只有一个140M信号输出。现在已经排除了电源、20M参考、AD9957内部PLL、AD9957的DDS的问题,不使用AD9957的PLL,直接输入640M参考也试过。这种现象只和PDCLK频率有关,频率越低会好很多,PDCLK频率越高越严重。总结就是杂散的严重程序只和PDCLK频率和温度有关。下图右是比如严重,左是特别严重的情况。

Parents Reply Children
No Data