ADA4895-1的问题

问题描述:

1、批次1917的芯片都不能用。

TEST2的波形图如下所示。在超声波信号到来的一段时间(将近33us内),波形是一条直线。33us后,噪声陡增。或者不放大超声波信号。

2、老的批次基本可以用。

请问这种现象是因为芯片的原因还是使用的原因造成的?

Parents
  • 0
    •  Analog Employees 
    on Oct 10, 2019 9:13 AM over 1 year ago

    1. 请检查Disable引脚的电平是否符合Datasheet的需求;

    2. 如果只从33us开始出现问题,请检查一下电路中哪个信号的触发点与此时间相吻合,运放如果有问题,会一直有问题,而不会存在一个时间差。

    3. 可以将供电的电阻4.7R去掉,因为此输入信号是高频信号,供电引脚的输入阻抗,可能会对输出有影响。

  • 谢谢答复。可以确定的事情:1、Disable引脚符合Datasheet要求;2、在这个时刻只有示波器黄线那个触发信号,这个是超声换能器的驱动信号。3、频率并不高。4.7R去掉也是这样。

    对比测试是在同一块电路板上进行的。只是替换不同批次的ADA4895-1。

  • 0
    •  Analog Employees 
    on Oct 15, 2019 2:20 AM over 1 year ago in reply to DAVID1077

    如果要确定运放的问题,可以只保留同相放大电路,输入用信号源,输出用示波器,来检查两个批次的运放是否有异。如果没有差异,说明是运放应用的问题,可以在你的电路中,调节一下运放输入端的阻抗看一看变化(R77,R73,R83,R63,R84和R85,优先考虑先拆掉R77看一下效果)。示波器是不能加在运放的输入端的测试的,因为示波器本身有1MR的内阻,这样与运放输入端的高内阻等效并联,使运放等效内阻降低(所以R77可以拆掉调试一下),会影响输出。把示波器放在低阻位置(运放输出端)测试。

Reply
  • 0
    •  Analog Employees 
    on Oct 15, 2019 2:20 AM over 1 year ago in reply to DAVID1077

    如果要确定运放的问题,可以只保留同相放大电路,输入用信号源,输出用示波器,来检查两个批次的运放是否有异。如果没有差异,说明是运放应用的问题,可以在你的电路中,调节一下运放输入端的阻抗看一看变化(R77,R73,R83,R63,R84和R85,优先考虑先拆掉R77看一下效果)。示波器是不能加在运放的输入端的测试的,因为示波器本身有1MR的内阻,这样与运放输入端的高内阻等效并联,使运放等效内阻降低(所以R77可以拆掉调试一下),会影响输出。把示波器放在低阻位置(运放输出端)测试。

Children
No Data