按照用户手册描述,连接完电源后CR3会亮,然后连接了USB接口以后,应该CR3会闪烁,然后电脑与开发板连接成功。但是我早上的评估软件崩溃了一次以后,再连接USB接口,CR3仍旧常亮不闪烁,检查用户手册上提到的P3.P10.P9及USB接口都没有问题,事实上上一次使用的时候还是正常的,但是这一次开机后原样连接却再也连不上了,想问问这是怎么了。我也没想出来有什么导致板子坏掉的可能性,毕竟是个新板。
附用户手册上的指南:
If the green CR3 LED is not blinking, ensure that:• Jumpers are installed on Position P2 and on either the I2C or the SPI position of P3 and P10.• The jumper on P9 lies across the center pin and the PC symbol.• The USB port on the PC is operational and that the USB cable is not damaged.
事实上就算跳线不在P2或者P3.P10上,CR3也常亮,和连上没有任何区别。
您好,请将您的问题发布在咱们的全球技术社区哦ez.analog.com/.../