工业4.0的关键在于从工厂车间边缘收集数据,为工厂控制器提供有价值的洞察,帮助工厂做出更明智或“更智慧”的决策。此外还让制造商能够快速轻松地定制产品,而无需为重新配置制造流程付出大量成本。这就打开了“单件小批量生产”制造流程的大门,有助于减少浪费,让工厂生产更加可持续。IO-Link在实现工业4.0方面扮演着重要角色,不仅适用于新工厂,而且还能轻松升级现有老旧设施。近年来,IO-Link节点的数量呈指数级增长,预计这种增长趋势将持续发展。这篇博文探讨IO-Link为追求智能化流程的制造商带来的三大关键优势。下方的图1显示了IO-Link的增长率。

图1.IO-Link节点安装数量不断增加
- IO-Link将智能引入边缘
IO-Link为工厂车间边缘的传感器和执行器提供高达230kbps的双向数字数据通信接口,使其能够测量、监控和控制生产线的各个阶段。边缘处理的决策越多,需传输到控制室PLC的数据就越少,从而能够有效节省时间和能源。例如,除了C/Q数据线之外,传感器还可以使用IO-Link接口中的引脚2 (I/Q)作为数字输出(DO),读取来自二进制传感器的输入信号,并同时驱动LED指示超过阈值的情况,而无需用户输入来做出此决策。下方图2为典型IO-Link传感器的框图。

图2.IO-Link传感器的构建模块
- IO-Link支持简化安装
IO-Link使用标准化接口,用工业环境中普遍使用的便捷M12连接器取代了传统的模拟、二进制和串行接口。此外,该接口采用标准非屏蔽布线安装方式(例如图3中带M12连接器的3芯非屏蔽IO-Link电缆),因此升级设施以使用IO-Link的成本很低。IO-Link还向后兼容串行输入/输出(SIO)二进制信号,也就是说支持IO-Link的传感器可以使用标准数字输入通信通道与现有PLC进行通信。PLC模块升级为与IO-Link主站连接后,IO-Link通道上的C/Q线路就可以与工厂车间的设备进行双向通信。IO-Link与现场总线类型无关,可以在各种工业网络架构中无缝使用。

图3.IO-Link电缆
- IO-Link有助于减少维护并增加正常运行时间
IO-Link有助于确保实时诊断信息畅通无阻,让工程师可以及时发现并迅速解决问题,防患于未然,同时让技术人员也能快速更换故障传感器。支持IO-Link的设备具有自主调试和自动设置参数的功能,从而能够进一步简化上述任务的操作过程。在许多情况下,技术人员可以从控制室远程执行配置更新,无需前往工厂车间。举个例子,需调整生产线以生产不同产品时,技术人员可以实时重新配置相关工艺参数,从而尽可能缩短停机时间,加速恢复全面生产。下方图4为距离传感器的参考设计,例如用于测量传送带上物体尺寸的距离传感器。然而,与传统传感器不同的,如果需要更改物体尺寸的公差,可以通过远程控制修改该IO-Link传感器测量距离。

图4.MAXREFDES174:IO-Link距离传感器
Edit Notes
修订[edited by: Admin_ADI at 2:14 AM (GMT -5) on 30 Jan 2024]