Post Go back to editing

官方音频总线(A²B)资料包免费放送中,赶紧来领取啦~

随着汽车智能网联化的发展,对音频的开发要求也越来越高,ADI通过对音频总线的优化,推出A2B(Automotive Audio Bus)车载音频总线,能比传统模拟音频总线能够提供出色的音频质量,同时还能大大节省汽车音频线束重量和成本(约减少75%)。

那么A2B实现模式如何,有着怎样的生态系统,应用实例又有哪些?斑竹为感兴趣的各位小伙伴整理了关于A2B 音频总线的相关课程及资料,赶紧扫码下载吧!

Parents
  • 课程——A2B:更好的音频设计体验

    ADI的A2B技术是一种简化音频设计并提供解决诸多挑战的方法,如降低布线成本、复杂度和重量。A2B具有可配置的44.1或48 kHz帧速率以及高达50 Mbps的带宽,非常适合传输数字音频,提供相对于模拟连接的出色音频质量和低延迟性能。A2B正在解决汽车、智能楼宇、消费电子和新兴应用领域的问题。本次课程将介绍以下内容:

    • 什么是A2B及其为音频系统带来的价值

    • A2B生态系统见解

    • A2B的示例应用

  • 请问2428是否支持16个通道数据输入?通过PCM /IIS 数据输入,或是否有方法支持 ?是否有实际案例参考

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.