Post Go back to editing

使用EVAL-AD428WD1BZ demo板下载ADI_A2B_Software-Rel19.4.5例程的SS工程,提示版本不匹配

Thread Summary

The user encountered a version mismatch when trying to download the ADI_A2B_Software-Rel19.4.5 example SS project to the EVAL-AD428WD1BZ demo board. The solution involves checking the SS User Guide for version switching and ensuring the board is configured to boot from EEPROM (JP4). The EVAL-AD428WD1BZ user guide and QuickStartGuide are available in the SS installation directory, and the SS schematic only configures A2B, with the ADAU1761 codec configured automatically at power-up.
AI Generated Content

Hi ,

   有几个问题想要请教一下,谢谢~

    1. 我使用EVAL-AD428WD1BZ demo板下载ADI_A2B_Software-Rel19.4.5例程的SS工程,提示版本不匹配,例程路径如下:

C:\Analog Devices\ADI_A2B_Software-Rel19.4.5\Schematics\BF\A2BSchematics :  adi_a2b_3NodeSampleDemoConfig

Demo板拿到以后我只给板子做了12V供电和连接USBi的动作,其他部分没动过

    2. EVAL-AD428WD1BZ这个demo板是否有资料讲解如何使用?有的话能否提供一下相关的文档

    3. EVAL-AD428WD1BZ 这个demo板的pcb我打不开,请问是否有对应的导出pdf文件可以用来查测试点,谢谢~

    4. EVAL-AD428WD1BZ 使用USBi下载工程,是使能DSP芯片还是DSP+A2B+1761芯片?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.