用STM32的FSMC控制LCD的一些疑惑

* Description        : This file includes the LCD driver for AM-240320L8TNQW00H

*                     (LCD_ILI9320) Liquid Crystal Display Module of STM3210E-EVAL

*                      board.

//////////////////////////////////////////////////////////////////////////////////////

/* Private typedef -----------------------------------------------------------*/

typedef struct

{

  vu16 LCD_REG;

  vu16 LCD_RAM;

} LCD_TypeDef;

/* LCD is connected to the FSMC_Bank1_NOR/SRAM4 and NE4 is used as ship select signal */

#define LCD_BASE    ((u32)(0x60000000 | 0x0C000000))

#define LCD         ((LCD_TypeDef *) LCD_BASE)

////////////////////////////////////////////////////////////////////////////////////////

void LCD_WriteReg(u8 LCD_Reg, u16 LCD_RegValue)

{

  /* Write 16-bit Index, then Write Reg */

  LCD->LCD_REG = LCD_Reg;

  /* Write 16-bit Reg */

  LCD->LCD_RAM = LCD_RegValue;

}

/////////////////////////////////////////////////////////////////////////////////////////

u16 LCD_ReadReg(u8 LCD_Reg)

{

  /* Write 16-bit Index (then Read Reg) */

  LCD->LCD_REG = LCD_Reg;

  /* Read 16-bit Reg */

  return (LCD->LCD_RAM);

}

/////////////////////////////////////////////////////////////////////////////////////////

void LCD_WriteRAM_Prepare(void)

{

  LCD->LCD_REG = R34;

}

/////////////////////////////////////////////////////////////////////////////////////////

void LCD_WriteRAM(u16 RGB_Code)

{

  /* Write 16-bit GRAM Reg */

  LCD->LCD_RAM = RGB_Code;

}

这是例程里lcd.c里的一下底层函数的实现。在结构体里的定义:LCD_REG变量地址:0x6c000000;

LCD_RAM变量地址:0x6c000001,STM32的FSMC的地址引脚A0接LCD_ILI9320的RS(L:访问reg;H:访问ram) ,

通过给LCD_REG变量或LCD_RAM变量写数据来实现访问reg和ram,是这样理解的吗?

那么为什么在写LCD_ILI9320的寄存器时,函数 LCD_WriteReg(,)里对reg写操作:LCD->LCD_REG = LCD_Reg;先发送reg的编号,

再 LCD->LCD_RAM = LCD_RegValue; 为什么是对LCD_RAM赋值来实现发送reg需要修改的数据啊?不懂。

还有 LCD_ReadReg(u8 LCD_Reg)的读操作,

也不大明白,怎么实现的啊?

对LCD_ILI932里的reg,ram读写操作时,要给/WR(写入),/RD(读入) 信号的,在用FSMC模块时,程序里没涉及到这些读写信号啊?

高手指点下在下啊?FSMC控制LCD_ILI9320是个什么过程啊?小弟不胜感激!