ADN8831做温度控制,问题供电电源跳动很大,请教指点下,谢谢!

接上TEC和NTC热敏电阻,上电后,5V20A的供电电源一直跳动,变化范围为3.7V-4.7V之间,很奇怪,参考电压输出2.41V,灯间断闪烁,设定电压1.44V,热敏电阻输出电压0.63V-0.73V,不稳定,麻烦知道的指导下,非常谢谢。附件是原理图。

Sheet1.pdf
Parents
No Data
Reply
  • 最近也是遇到同样的问题,用的TEC制冷片最大电流才2A,用台式稳压电源供电,稳压电源电流限制在4A,上电后,电流1A不到,一会就开始过流,超过4A,这时台式电源输出电压跳动(限流4A的原因),这个时候ADN8831会发热烧毁。也就是超过4A的电流,不合理。什么原因?我怀疑是PID环路不适合导致输出震荡。难道电流供电电流要超过4A?为什么PID不合适就损坏芯片,那不是调PID时候会烧很多芯片?

Children
No Data