ADN8831输出电流太小,不知道是怎么回事?请求帮助!

ADN8831输出电流太小,不知道是怎么回事?

使用的电路是Datasheet给出的典型电路,芯片供电使用的是9V的蓄电池加一片LM1117降压为5V供电,但是输出电流为mA级别,根本无法驱动TEC工作。上电之后,Pin29(ITEC)的电压值为0.17V,Pin30(VTEC)的电压值为1.32V,Pin31(VLIM)的电压值为1.21V,Pin32(ILIM)的电压值为0.78V。有谁知道这是怎么回事吗?求解答,望不吝赐教。

  •      你这电路明显不合理啊,一般1117最多也就能输出几百mA吧,并不是8831输不出那么大的电流,实在是你的1117不给力啊,而且8831根本不需要大电流输出的,驱动那几个mos的栅极才需要多大的电流啊?

         你先测量一下你的1117输出电压是不是到不了5V(被拖下来了),估计你摸一下1117会有烤肉的味道

         最简单的方法你这个把1117换成ADP2303试一下,另外还有你需要估算一下你的TEC最大电流是多大,如果大于2.5A的话你可能需要更大的buck电源,有问题的话你继续发帖。

  • 您好!首先感谢您的答复。关于您的解答,这里有几个问题。1、1117输出电压确实为5V,工作正常,1117确实有点发热,但发热不明显;2、实际电路中,通过设定相应管脚的电压,TEC的制冷和制热的最大电流均限制为2A,另外,根据同事的说法,TEC一般工作的电流需要达到安培A级别,所以认为8831经过MOS管之后正常应该输出较大的电流;3、根据您的解答,是不是说,8831的供电电源除了有合适的电压,还应该有合适的电流,也就是电源应该有个合适的功率,不知这样理解是否准确?4、根据Datasheet,19管脚的作用是PWM输出驱动MOS管工作(“PWM Output Drivers External PMOS Gate ”),但是实际测出来只是一个高电平,没有看到任何波形,不知这是为何?5、在这样的接法中,发现MOS后面接的4.7uH的电感会发烫,其他的元件都正常;6、电源地和模拟地之间接了电感作为隔离,不知是否对电路有影响?

  • 谢谢。现在上电之后TEC正负之间的电压只有0.1V到0.2V,电流几十毫安,这样能驱动TEC正常工作吗?感觉TEC没有工作。

  •      8831实际上需要的电流很小的,最多就是几十mA的样子,主要的TEC电流都是从LPGATE和SPGATE接的那两个MOS上面流过去的,你要注意这两个MOS的电源必须要和8831是同一个电源才行。

         你说的PWM输出只是一个高电平说明8831还没有稳住温度呢,你的4.7uH是什么电感啊?可不能是0805那一类的贴片电感啊,必须用超大电流功率电感。你做实验的时候可以先把模拟地和数字地直接短路。

  • 你看看你的MOS管都工作了吗?8831的各个驱动脚是什么波形?你用的MOS管是对管吗?