我是南方科技大学的一名本科生,目前正在使用 ADA4530-1 搭建有源积分器,用于微弱双向电流检测。在实际调试过程中遇到了积分器输出快速饱和至电源轨的问题,因此想向您请教几个相关问题。
目前电路参数如下:
- 运算放大器:ADA4530-1
- 供电电压:±6 V
- 期望输出线性范围:约 ±4.3 V(受后级 ADC 输入范围限制)
- 反馈网络:仅使用 30 pF 电容(Cf = 30 pF),未并联反馈电阻
- 参考电流:ADG1219 模拟开关输出 ±5 V 方波,经 100 MΩ 电阻产生约 ±50 nA 电流
- 被测电流:双向微弱电流,目标量程约为 ±50 nA
- 两路电流在运放反相输入端汇合并进行积分
目前观察到的现象是:上电后不足 1 s,ADA4530-1 的输出便迅速饱和至约 ±5.9 V,已经非常接近 ±6 V 的供电轨。同时,输出最终饱和的极性并不完全固定,偶尔会出现由正轨跳变至负轨或相反的情况。
我了解到,在纯电容反馈的积分器中,微小的输入失调电流、输入偏置电流或初始电荷都可能持续积累并最终导致输出进入饱和。因此,我目前最想确认的是:
在使用 ADA4530-1 测量 pA~nA 级电流的情况下,仅采用反馈电容而完全不设置直流反馈通路,是否适合长期工作?如果需要额外的复位或泄放机制,一般推荐采用什么方式?
此外,我参考了一篇相关论文中的实物电路,发现其与我的设计相比存在两个差异,但论文没有标注具体阻值。由于无法确定这两个电阻的实际设计目的,因此希望向您请教。
- 在信号源输出端与运放反相输入端之间串联了一个电阻(附件/图片中的位置 A)。
请问这种电阻通常承担什么作用?是用于限制开关切换瞬间的电流、提高积分器稳定性,还是与输入阻抗或其他寄生参数有关?其阻值一般应如何确定?
- 在运放同相输入端与地之间连接了一个电阻(图片中的位置 B)。
在双电源供电条件下,如果同相输入端需要作为 0 V 基准,直接接地与通过一个电阻接地分别有什么差异?该电阻是否可能用于输入偏置电流补偿或其他目的?
另外,由于我的电路涉及 pA~nA 级微弱电流,我也想进一步了解:上述电阻如果确实需要使用,在元件选型时是否需要特别关注材料和结构,例如表面漏电、吸湿性、绝缘电阻、热电势以及电阻噪声等?对于这种应用,普通厚膜贴片电阻是否可能带来明显问题,是否更建议使用金属膜、薄膜或其他类型的电阻?
如果您方便的话,非常感谢您能给我一些判断方向或推荐的参考资料。
感谢您的时间!
祝工作顺利!
江学斌
南方科技大学
Dear Wong,
I am an undergraduate student at Southern University of Science and Technology, and I am currently building an active integrator based on the ADA4530-1 for low-level bidirectional current measurement.
During the initial testing of the circuit, I encountered a problem where the integrator output rapidly saturates near the supply rails. I would therefore like to ask for your advice regarding several aspects of the circuit design.
The main circuit parameters are as follows:
- Operational amplifier: ADA4530-1
- Supply voltage: ±6 V
- Expected linear output range: approximately ±4.3 V, limited by the input range of the following ADC stage
- Feedback network: a single 30 pF capacitor (Cf = 30 pF), with no resistor connected in parallel
- Reference current: a ±5 V square-wave signal generated through an ADG1219 analog switch and converted into approximately ±50 nA through a 100 MΩ resistor
- Measured current: bidirectional low-level current with a target range of approximately ±50 nA
- The reference current and the measured current are summed at the inverting input node of the operational amplifier and integrated
The problem I observe is that, after power-up, the ADA4530-1 output saturates to approximately ±5.9 V in less than one second, which is very close to the ±6 V supply rails. The final saturation polarity is not always consistent, and the output occasionally changes from one supply rail to the other.
My understanding is that, in an integrator with purely capacitive feedback, very small DC errors, such as input offset current, input bias current, leakage current, or initial charge on the feedback capacitor, may accumulate continuously and eventually drive the output into saturation.
Therefore, my main question is:
For pA-to-nA level current measurement using the ADA4530-1, is it practical to operate the integrator with only a feedback capacitor and no DC feedback path? If some form of reset or discharge mechanism is required, what implementation would generally be recommended?
In addition, I found two differences between my circuit and a physical circuit shown in a related paper. The paper does not provide the values or detailed purposes of these components, so I would like to ask for your opinion.
- A resistor connected in series between the signal source output and the inverting input (-IN) of the amplifier (position A in the attached figure).
What is the typical purpose of such a resistor? Could it be used to limit transient current during switching, improve the stability of the integrator, or control the interaction with input impedance and parasitic capacitance? How would its resistance value normally be determined?
- A resistor connected between the non-inverting input (+IN) and ground (position B in the attached figure).
Under dual-supply operation, if the non-inverting input is intended to use 0 V as its reference, what is the difference between connecting it directly to ground and connecting it to ground through a resistor? Could this resistor be related to input bias current compensation or another design consideration?
Finally, since this circuit involves pA-to-nA level current measurement, I would also like to ask whether special considerations are required when selecting these resistors. For example, should parameters such as surface leakage, moisture absorption, insulation resistance, thermoelectric effects, temperature coefficient, and noise be carefully considered?
Would a standard thick-film surface-mount resistor potentially introduce noticeable errors in this application, or would thin-film, metal-film, or another resistor technology be more appropriate?
If convenient, I would greatly appreciate any guidance or references that could help me better understand the design considerations.
Thank you very much for your time and assistance.
Best regards,
Jiang Xuebin
Southern University of Science and Technology