Post Go back to editing

双源输入储能电路,电磁振动、温差能量的收集

Category: Hardware
Product Number: ADP5091ACPZ-2-R7, ADP5091, ADP5091

     按照手册,分压电阻设定的温差支路电容放电阈值为3.9V,实际在小于3.4V时开关就被导通,电池与电容直接并联,在输入1.9~2.2V的情况下开路电压最高为3.560V,远达不到预期,目前还未进行电磁支路的测试,稳定时SYS电压与BAT接近,SETPG电压为1.1V左右,TERM电压为1.03V左右,不知问题出在哪里

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.