Post Go back to editing

Request for AD9653 and HSC-ADC_EVALC FPGA configuration files

Category: Hardware

VisualAnalog: Increasing AD9253 output data sample length doesn't seem to work past 65536 - Q&A - High-Speed ADCs - EngineerZone

Hello, I recently purchased the AD9653 evaluation board.
In this discussion, I learned that the maximum data length supported by the software for the AD9653 evaluation board is 65536. I have two questions:
1. Where can I obtain the HSC-ADC_EVALC FPGA configuration files?
2. If the DDR is configured, can VisualAnalog support the collection of more than 65536 data points?

Thread Notes

Parents Reply Children
No Data