Category: Software
Product Number: AD9680
我现在用fpga jesd204b子类1+ad9680采集数据,fpga是xilinx7z035,子类1模式下,目前配置不同速率测试,均发生了周期断链现象,如输入时钟312.5M(fpga和adc同源同频),L=2,线速率6.25Gbps;还有输入时钟500M,线速率10G都是在约0.5ms左右发生断链,从vivado里查看是GT_PLL_LOCK断链,约113个core周期后,GT_PLL_LOCK自动恢复。并且子类0下也测试了,sync信号发出后也是采集数据很快就断链了,说明和sysref信号无关。目前发现pcb板图上时钟进入adc和fpga的走线长度不一致,外接时钟是先进入adc芯片,之后再经过约10cm之后进入fpga时钟pin脚,,这个断链和pcb设计里时钟走线有关系吗?如果有关系是什么原理?还是其他原因导致的?感谢大佬支持