Post Go back to editing

AD9910参考时钟输入后PLL没办法锁定

Category: Hardware
Product Number: AD9910

我用FPGA驱动AD9910没办法锁定PLL到1GHz。(PLL_LOCK引脚一直是低电平,REFCLK_OUT有时钟信号)
我用了50MHz外部有源时钟,但之前降压没计算好,REFCLK输入大于1000mvpp,后来发现问题后降压到700mVpp。
计算环路滤波电路,根据计算公式,我采用分频系数N=20,鉴相器增益KD=387uA,VCO增益KV=850MHz/v,开环带宽fOL=200kHz,相位裕量0.785(45°),得出R1 ≈ 92.25 Ω,C1 ≈ 20.81 nF,C2 ≈ 4.32 nF。
设置CFR3寄存器也使能了PLL标志位。我的串行通讯设置没有问题,可以正常初始化设置,但因为没法锁定时钟,导致我输出5MHz正弦信号实际只有3.5MHz。
请问问题出在了哪里呢。

Thread Notes

Parents Reply Children
No Data