Post Go back to editing

关于如何外接防反接保护PMOS(Regarding how to externally connect a PMOS for reverse-polarity protection.)

Category: Hardware
Product Number: MAX17525

MAX17525外部防反接PMOS是如何连接的?是D级连接芯片输入引脚还是S级连接芯片输入引脚?官方手册给出的参考电路图,外部防反接PMOS是S级连接芯片输入引脚,该参考图纸是否是防反接功能?
How is the external reverse-polarity protection PMOS connected for the MAX17525? Is the Drain (D) connected to the chip's input pin, or is the Source (S) connected to the chip's input pin? In the reference circuit diagram provided in the official datasheet, the external reverse-protection PMOS has its Source (S) connected to the chip's input pin. Does this reference schematic actually provide reverse-polarity protection?

Thread Notes