Post Go back to editing

MAX17577芯片24V转-5V,空载或带电阻都工作正常,但是驱动陀螺时芯片不工作。

MAX17577芯片24V转-5V,空载或带电阻都工作正常,但是驱动陀螺时芯片不工作,输出0.1V,led指示灯不亮。芯片没有坏,只要断开陀螺工作就正常。陀螺的启动电流很小,用直流电源测试只需小于0.1A的电流即可启动,17577芯片带电阻工作时测试到输出0.5A仍工作正常,应该不是电流不足。目前输出电容为44uf的钽电容以及手册上推荐的0.1uf等电容。想问该情况出现可能是什么原因呢?