Post Go back to editing

AD9912评估板输出频率错误

Category: Hardware
Product Number: AD9912

测试环境:使用外部10MHz恒温晶振为AD9912评估板提供时钟,设置内部时钟2倍频,设置Multiplier位40,也就是将10MHz倍频80倍,最后系统时钟为800MHz,当我设置输出频率为10MHz时,使用频率计测试得到频率为13.999993MHz,大约是设置频率得1.4倍

评估板软件设置如下图所示

频率计测试如下图所示

再将输出信号接到示波器看,会发现有很多条迹线

将CLKMODESEL接到VDD和GND都试过,都是这样的结果,找了很久不知道是什么原因。设置电荷泵电流时输出信号的频率也会改变,后来直接使用射频源输出1GHz信号当做评估板输入时钟,将AD9912内部Clock Multiplier旁路掉,这时候输出频率是准的,猜测是AD9912内部VCO的问题,导致系统时钟不准,所以导致输出频率错误,求各位专家解惑

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.