Post Go back to editing

ad6676 输入-47dBm单音时,输出饱和

Category: Datasheet/Specs
Product Number: ad6676

测试AD6676时,发现以下现象。

测试条件是,

1)自研单板,AD6676+XC7K325T,AD6676 VIN±只有0.01uf隔直电容
2)配置使用clock synchronizer,参考122.88MHz;FADC = 2949.12MHz,decimation factors = 24,FDATA_IQ = 122.88M;FIF = 250 MHz, BW = 60 MHz
配置IDAC1FS = 4mA,衰减 = 0dB
3)信号源SMU200A,输出250.2MHz,幅度-47dBm,直接连接在VIN+


测试结果

1)204B接口正常
2)读取IQ数值,有正弦波,但峰顶发现已经有溢出现象,如下图

3)-47dBm远小于配置的-2dBm的dBFS,可能是什么原因?

Thread Notes