Post Go back to editing

MAX31790ATI+T寄存器读写相关问题

Category: Datasheet/Specs
Product Number: MAX31790ATI+T

测试MAX31790ATI+T的寄存器读写时遇到如下问题:

1、硬件上slave地址0x20的芯片FAN1连接实际风扇5, 芯片初始状态风扇为pwm模式,占空比读写正常。

2、pwm模式设置FAN1占空比为20%,然后将FAN 1 Configuration寄存器写入0xc9,风扇修改为rpm模式,此时读取TACH 1 Count寄存器18h、19h为0x0560,转换rpm值22891,风扇5变为满转。

3、修改控制风扇转速的TACH 1 Target Count寄存器50h、51h为0x07FF或其他值,读取寄存器18h、19h始终为0x0560,无法控制风扇的转速。

 

是否为rpm模式风扇转速控制存在问题,如何排查方向。如何确认MAX31790芯片风扇rpm模式始终满转的原因,以及是否可以提供rpm模式下控制风扇转速的方法,谢谢。

Thread Notes

Parents Reply Children
No Data