Post Go back to editing

能否提供ad9986 的fpga工程

Category: Hardware
Product Number: AD9986

adi专家你好

我申请了ad9986的api,但是只有软件部分,不知道对应的fpga工程在哪里可以找到,硬件环境应该是ADS9-v2EBZ,应该是xc7z020+ku5p的一个架构,软件和硬件是要配合上的,很多寄存器地址找不到对应的硬件

比如说下面的代码,应该是基于linux的,对应了四个设备,那这四个设备具体是什么IP,搞不清楚,不知道和HDL里面的工程有什么联系没有,HDL的工程里只有AD9081的project,不知道是否通用

static int32_t ads9_spi_open(void)
{
    int32_t err = API_CMS_ERROR_ERROR;
    g_spi_ctrl_fd    = open(SPI_CONTROLLERDEV, O_RDWR);
    g_spi_cs_fd      = open(SPI_CHIPSELECTDEV, O_RDWR);
    g_axi_jesd204_fd = open(AXI_JESD204DEV, O_RDWR);
    g_i2c_ctrl_fd    = open(I2C_CONTROLLERDEV, O_RDWR);
    if ((g_spi_ctrl_fd > 0) && (g_spi_cs_fd > 0) && (g_axi_jesd204_fd > 0) && (g_i2c_ctrl_fd > 0)) {
        g_spi_ctrl_mem    = mmap(NULL, SPI_CONTROLLERSIZE, PROT_READ | PROT_WRITE, MAP_SHARED, g_spi_ctrl_fd, 0);
        g_spi_cs_mem      = mmap(NULL, SPI_CHIPSELECTSIZE, PROT_READ | PROT_WRITE, MAP_SHARED, g_spi_cs_fd,   0);
        g_axi_jesd204_mem = mmap(NULL, AXI_JESD204SIZE,    PROT_READ | PROT_WRITE, MAP_SHARED, g_axi_jesd204_fd, 0);
        g_i2c_ctrl_mem    = mmap(NULL, I2C_CONTROLLERSIZE, PROT_READ | PROT_WRITE, MAP_SHARED, g_i2c_ctrl_fd, 0);
        if ((g_spi_ctrl_mem == MAP_FAILED) || (g_spi_cs_mem == MAP_FAILED) || (g_axi_jesd204_mem == MAP_FAILED) || (g_i2c_ctrl_mem == MAP_FAILED)) {
            printf("UIO mmap error.\r\n");
        }
        else {
            printf("UIO mapping address: 0x%x, 0x%x, 0x%x, 0x%x.\r\n", (int)g_spi_ctrl_mem, (int)g_spi_cs_mem, (int)g_axi_jesd204_mem, (int)g_i2c_ctrl_mem);
            err = API_CMS_ERROR_OK;
        }
    }
    else {
        printf("UIO device cannot be opened.\r\n");
    }
    return err;
}
我的邮箱是whxiao@wennyfly.com,如果能把fpga的工程发给我参考下这就容易多了,谢谢!

Thread Notes

Parents Reply Children
No Data