Post Go back to editing

The AD5940_BATImpedance Keil project for the EVAL-AD5941BATS evaluation board is not running correctly.

According to the process provided by CN0510 Circuit Note | Analog Devices, I downloaded the official Keil project from GitHub and compiled it, and then downloaded it to my device. However, the sample program AD5940_BATImpedance did not run successfully. Whether I made modifications according to CN0510 User Guide [Analog Devices Wiki] or not, I got the same wrong data. The official GUI can be used normally. I am sending you my hardware connection diagram and serial port data as attachments. I hope you can give me some help. I would be extremely grateful.
//*******************************************************//
[15:55:41.314]IN←◆Hello AD5940-Build Time:15:55:18
This AD594x!
Note: Current Silicon is S2
AD5940LIB Version:v0.2.1
[15:55:49.386]IN←◆i: 1   Freq: 1.00  RcalVolt:(38154.605469,8490.803711)
[15:55:49.494]IN←◆i: 2   Freq: 1.25  RcalVolt:(0.000000,0.000000)
//*******************************************************//
The error log is already included in the attachment. What I need help with is how to obtain 50 scan data points from the serial port. I would greatly appreciate your response!
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.