Post Go back to editing

The AD5940_BATImpedance Keil project for the EVAL-AD5941BATS evaluation board is not running correctly.

According to the process provided by CN0510 Circuit Note | Analog Devices, I downloaded the official Keil project from GitHub and compiled it, and then downloaded it to my device. However, the sample program AD5940_BATImpedance did not run successfully. Whether I made modifications according to CN0510 User Guide [Analog Devices Wiki] or not, I got the same wrong data. The official GUI can be used normally. I am sending you my hardware connection diagram and serial port data as attachments. I hope you can give me some help. I would be extremely grateful.
//*******************************************************//
[15:55:41.314]IN←◆Hello AD5940-Build Time:15:55:18
This AD594x!
Note: Current Silicon is S2
AD5940LIB Version:v0.2.1
[15:55:49.386]IN←◆i: 1   Freq: 1.00  RcalVolt:(38154.605469,8490.803711)
[15:55:49.494]IN←◆i: 2   Freq: 1.25  RcalVolt:(0.000000,0.000000)
//*******************************************************//
The error log is already included in the attachment. What I need help with is how to obtain 50 scan data points from the serial port. I would greatly appreciate your response!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.