Post Go back to editing

ADBMS1818大储系统AFE首末节出现采集跳变

Category: Hardware
Product Number: ADBMS1818
1500V大储系统应用,配套1750kW PCS运行中,偶发性出现单体电压采集跳变问题,2种共同现象:
1.充电或放电过程中,AFE第一节或最高节突然向下跳变20mV-500mV,有些可以自行2-5分钟恢复,有些无法恢复需要插拔采集连接器,相当于给AFE重新上电才可以恢复;
2.充放电循环过程中,AFE第一节或最高节每个充放电过程中下降10-20mV,经历5个循环后整体偏差接近50-100mV,而且此节整体充放电过程电压变化趋势都是正确,除非插拔采集连接器否则无法发现采集偏差已经达到50-100mV;
 
已经排除线束、连接器接触问题,3次挑选无法自行恢复AFE,测量到Cn-Cn-1前端的电容全部为正确的电池电压(并不存在与其他节大幅度50mV偏差),但AFE采集值始终偏差存在,重新插拔采集连接器恢复正常;
 
5个集装箱大约1500片1818,充放电经历20个循环已经出现15次不同集装箱不同电池簇的采集问题。
目前与原厂FAE多次沟通无法解决问题。

Thread Notes

Parents Reply Children
No Data